News & Infos

Long-Running Precision
If precise, quiet and dynamic linear movements are required, linear guide rail systems are indispensable. For special applications, Ganter has now…

Stability Perfected
Machines and systems always require stability. Heavy duty, large size element also emphasize the quality of the objects they support. Ganter has added…

Reliable and Corrosion-Resistant
Ganter continues to expand its selection of standard parts of A4 stainless steel – now including threaded plugs, magnetic plugs and robust oil sight…

Perfect Latching
Wherever something needs to be adjusted, you will often find locking joints at work with serrations that define specific angle positions. To ensure…

A Connection That Won’t Let Go
To reduce the time involved in setting up equipment and production lines, Ganter has incorporated a new coupling in its product portfolio. With the GN…

Universally and Securely Fastened
Many things that hardly draw notice are nevertheless of elementary importance within the overall context. For example, it would be hard to conceive…

Fast and Secure Closing
Toggle latches are proven and universal elements for fast and secure closing of covers and hoods. With GN 761, Ganter now offers exactly the right…

Spirit levels with adjustment and cross-measurement
In digital times, they seem like relics from the past, but spirit levels remain indispensable tools in everyday industrial operations. Two new spirit…

Stopping germs in their tracks
Contact infections with viruses, fungi and bacteria were already a problem even before the pandemic – and now Ganter is expanding its Sanline range of…

Perfectly positioned with stainless steel adjusting screws
On production machines and mechanisms, it is often necessary to carry out repeated positioning operations as simply and reliably as possible. For…