Gear Levers GN 210 Awarded the iF DESIGN AWARD and the RedDot Award 2026
Gear levers GN 210 serve as precise control elements for the positive transmission of torque to shafts. They are used in applications where mechanical functions such as gear shifting, engaging clutches, or actuating valves and locking mechanisms are required.
The product range is characterized by a clear industrial design and functional versatility. The levers feature a textured plastic coating available in black or silver. An ergonomic shape, simple installation, and a wide range of customization options enable their use in various applications in mechanical and plant engineering.
About the iF DESIGN AWARD
Since 1954, the iF DESIGN AWARD has been a globally recognized hallmark for outstanding design. The iF Design brand is internationally established as a symbol of excellence in design achievements. The iF DESIGN AWARD is one of the most important design prizes in the world.
It recognizes design achievements across all disciplines, including product, packaging, branding and communication, service design, architecture and interior architecture, as well as user experience (UX), user interface (UI), and professional concepts. All award-winning entries are presented on ifdesign.com.
About the Red Dot Award
The is one of the world’s most renowned design competitions and has been awarded since 1955. It is organized by the in Essen, Germany. The award recognizes products that demonstrate exceptional design quality, innovation, and functionality. The competition is divided into the categories Product Design, Brands & Communication Design, and Design Concept. Entries are evaluated by an international jury of experts according to clearly defined criteria. Award-winning products are presented in the Red Dot Design Museum and featured in yearbooks as well as on the official online platform.