JW Winco

Our customers in the USA are managed by JW Winco. Please, use the website of JW Winco: jwwinco.com

Standard parts with antibacterial surfaces

Handles and operating elements can act as vectors for many pathogens. Upon every hand contact, bacteria and germs take hold on the surface, where they can proliferate unchecked over time, such as between two cleaning cycles. If one or more other people later touch the same part, the expanded population of pathogens has the opportunity to spread even further.

The antibacterial standard parts of the Sanline product family can prevent bacteria and germs from propagating on an operating element, actively reducing their spread and preventing bacterial illnesses that could otherwise result.

Two different active principles can be found in the Sanline product family: Plastic standard parts with additives based on silver ions and metal standard parts with a powder coating based on zinc molybdate. Both principles destroy the cell walls of the microorganisms, causing them to die. The antibacterial effectiveness is retained for a long time, even after frequent cleaning cycles, and is absolutely safe for the user.

With their antibacterial properties, the Sanline operating elements are predestined for areas with elevated hygiene requirements. These include doctors’ offices, hospitals, rehabilitation and care facilities as well as cafeterias, food-processing plants and agricultural operations with livestock. Sanline products also reduce the risk of infection in locations where many different people come into contact with handles and operating elements, such as in stadiums and concert halls, parks and wellness facilities as well as on public transport.

Further information can be found on our Sanline special page.

Zurück

Ganter Pressemeldungen

Sie suchen Pressemeldungen zu Produktneuheiten oder Sortimentsertweiterungen?

Zu den Pressemitteilungen

Es ist ein Fehler aufgetreten!
Kontaktwunsch bestätigt! Wir melden uns.
Service-Telefon

Unser Service Team ist von Montag bis Freitag von 07:00 bis 17:30 Uhr erreichbar unter:

Rückruf anfordern
Ihr Ansprechpartner

Sie suchen eine Ganter-Vertretung in Ihrer Nähe? Bitte wählen Sie das gewünschte Land.